MOVE.VCMD

Description

MOVE.VCMD reflects the velocity commanded by the Trajectory Generator when DRV.CMDSOURCE = 5 (program) and DRV.OPMODE = 2 (position). MOVE.VCMD is only valid when DRV.CMDSOURCE = 5 (program) and DRV.OPMODE = 2 (position).

General Information

Type

R/O

Units

Depends on UNIT.VROTARY, UNIT.VLINEAR or UNIT.ACCLINEAR
Rotary: rpm, rps, deg/s, (custom units)/s, rad/s
Linear: counts/s, mm/s, µm/s, (custom units)/s

Range

N/A

Default Value

N/A

Data Type

Float

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1150

No 32 bit No

M_01-05-11-000

Related Topics

DRV.CMDSOURCE | DRV.OPMODE